Issue
Can I use the new STR500 Continuum Room Temperature Sensor on a Smart Sensor port?
Environment
Continuum Controllers
Cause
Need an extra temperature input and the Smart Sensor port is not being used.
Resolution
As well as the Smart Sensor, the Smart Sensor port can support 10Kohm temperature sensors. The STR500 is a 10Kohm temperature sensor for the Continuum controllers. It will work on the smart sensor port but will only be usable as a temperature input, it will not have the full Smart Sensor abilities.