Issue importing CSV file

Issue

CSV file that has been edited with Excel does not import.

There is not error given but the import has no effect.

Product Line

Andover Continuum

Environment

CyberStation

Cause

This problem can occur if the application used to edit the CSV file adds hidden characters.

Resolution

Make sure the file contains ONLY plain text.

If possible, used a simple text editor such as Notepad