Issue
The following message appears after approximately 30 seconds when you attempt to edit a Menta file from the system Plug-in.
Environment
Windows 7
Vista 5.1.5, 5.1.6 and 5.1.7
Cause
The login screen does not come to the forefront when required
Resolution
Use the ALT - Tab key combination to scroll through the open windows.
Select the logon screen and continue with the normal process.