Issue
Satchwell VZF 2-Port Flanged Valve Body requires replacement.
Environment
Satchwell
2-Port
Plug and Seat
Flanged
Valve Body
VZF1727 VZF 1727
VZF1777 VZF 1777
VZF1852 VZF 1852
VZF1902 VZF 1902
VZF1954 VZF 1954
Cause
Obsolescence of Satchwell VZF 2-Port Flanged Valve Body
Resolution
A number of alternative S-E 2-Port Flanged Valve Bodies are available to replace existing Satchwell VZF 2-Port Flanged Valve Bodies.
Suggestion 1
Replace Satchwell VZF 2-Port Flanged Valve Body with S-E VG221F 2-Port Flanged Valve Body of appropriate size
N.B.
Existing Satchwell Actuator installed on VZF 2-Port Flanged Valve Body may be retained for installation on replacement S-E 2-Port Flanged Valve Body. In such instances a S-E L9TVG Linkage Kit will additionally be required. Alternatively an Actuator from the S-E range of Actuators may be installed on the VG221F 2-Port Flanged Valve Body, in which case no additional Linkage Kit will be required.
Suggestion 2
Replace Satchwell VZF 2-Port Flanged Valve Body with S-E V222 2-Port Flanged Valve Body of appropriate size
N.B.
Existing Satchwell Actuator installed on VZF 2-Port Flanged Valve Body may be retained for installation on replacement S-E 2-Port Flanged Valve Body. In such instances a S-E L8TV Linkage Kit will additionally be required. Alternatively an Actuator from the S-E range of Actuators may be installed on the V222 2-Port Flanged Valve Body, in which case no additional Linkage Kit will be required.
IMPORTANT NOTE
It should also be noted that the face to face dimensions both of the S-E VG221F and V222 2-Port Flanged Valve Bodies differ to that of the Satchwell VZF 2-port Flanged Valve Body
Similarly, the centre line to bottom of third port dimensions both of the S-E VG221F and V222 2-Port Flanged Valve Bodies differ to that of the Satchwell VZF 2port Flanged Valve Body
As a result alterations to the pipework connected to the VZF 2-port Flanged Valve Body will be required.
- Details of the Satchwell VZF 2-port Flanged Valve Body may be viewed here.
- Details of the S-E VG221F 2 port Flanged Valve Body may be viewed here.
- Details of the S-E V222 2-port Flanged Valve Body may be viewed here.
- Details of the S-E L9TVG Linkage Kit may be viewed here.
- Details of the S-E L8TV Linkage Kit may be viewed here.