BAS2800+ - Can a USB to Parallel converter be used for the dongle.

Issue

Using a USB to Parallel converter for the dongle.

Product Line

Other

Environment

BAS2800+

BAS 2800+

BAS

Dongle

Parallel

USB converter

Cause

The dongle is not seen when using a USB to Parallel port converter.

Resolution

In spite of investigations into the use of a USB to Parallel port converter, the BAS dongle cannot be successfully read.

It is recommended, that should the BAS 2800+ terminal require replacing, then the new PC is purchased with an additional Parallel port card..

If the PC is acquired from another source, then the appropriate type of Parallel port card should be purchased and fitted.

Using "Google" and searching for Parallel port cards, will provide a large selection. For "Google" click HERE.