HID PIN Pad reader for I/NET Part Number

Issue

HID PIN Pad reader for I/NET Part NumberHID PIN Pad reader for I/NET Part Number

Product Line

TAC I/NET

Environment

I/NET Access Control

Cause

HID PIN Pad reader for I/NET and which part number to use?

Resolution

iPortal shows several PIN pad readers from HID (HID-6136CKD000214 HID-6136CKD000009) but only one works with I/NET. 

Here is a pdf document which helps to explain which part number works with I/NET. The 09 means the 8 bit blast which is required for compatibility. 


Want to use Pin Pad only without using the proxcard? The RK40  will do Prox only or Prox + Pin but not Pin only. Check LL article 7476 for Pin Only or for higher security Pin Only check LL article 7474.