Description in List View editing causes error

Issue

Description in List View editing causes error

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation 1.1.xxx

Cause

1. Enter a description in the List View. This can be for anything, I selected a folder in the following two screenshots.
2. Boiler1 Folder: Description is Boiler
3. Boiler2 Folder: Description is Chiller
4. Graphics Folder: Description is Chiller
5. When I cut Ctrl-X the Graphics description and them on down the list, (imagine I have a lot of folders or devices I am putting descriptions in) if I save when not in that field, the error below occurs. 

Resolution

Upgrade to StruxureWare Building Operation Workstation release 1.2.0.659 or higher.