Issue
When changing name of a trendlog in Vista will the name of the trendlog in the SQL server also change?
This is when using Vista 5.1.7 and have upgraded the SQL database.
Environment
TAC Vista 5.1.7
Cause
The name of the trendlog in the SQL database will change when the next value for that trendlog is written in to the SQL database.
Resolution
The name of the trendlog in the SQL database will change when the next value for that trendlog is written in to the SQL database