Issue
What is the accuracy of the I/A Series MN-SX S-Link wall sensors? This information is required for submittal purposes.
Environment
MN-SX
MN-S1
MN-S2
MN-S3
MN-S4
MN-S4-FCS
MN-S5
S-Link
Cause
Published sensor accuracy information required for project submittal
Resolution
TPA-RKFD-09-0021.00 details sensor accuracy and stability as shipped from the factory and states:-
Element Type: Precision Thermistor
Operating Temperature Range: 0 – 50 °C (32 to 122 °F)
Stability: < 0.02 °C (< 0.04 °F) per year, typical
Accuracy
Temperature °C | Accuracy | Temperature °F | Accuracy |
24 °C | ± 0.6 °C | 75 °F | ± 1.0 °F |
0 to 50 °C | ± 1.7 °C | 32 to 122 °F | ± 3.0 °F |