Issue
Can photos be added to personnel using webclient?
Environment
Continuum
Webclient
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Webclient is mainly a viewer and doesn't have the ability with some features for editing.
There isn't a way from a Webclient browser PC to add or edit photos for personnel.
Resolution
Personnel photos must be added using Cyberstation personnel editor or personnel manager and may then be viewed in a webclient browser session.