Issue
Are the trendlogs in the Xenta deleted when downloading a Menta application?
Environment
- Vista 5.1.7
- Menta 5.1.7
- Xenta programmable controllers
Cause
When performing system updates to the either the logic of a Xenta programmable controller, or the firmware, it is important to know which of these actions will affect the stored Xenta trend log information inside the controller.
Resolution
- Downloading a Menta application to a Xenta does not affect the trendlogs. They are saved in the Xenta.
-
Downloading a Xenta firmware revision will delete all trend log data.