Issue
Net Controller time is off by 5 hours.
Environment
Continuum LAN and StandAlone
Cause
Network object UTC offset did not match the Net Controller UTC offset.
Resolution
Ensure the Network object UTC offset matches the Net Controller UTC offset when both are in the same time zone. Right click on the Network object in the Cyberstation Object Tree to set the Network