SysManSMS Server running in a Marathon EverRun Level 3 Solution?

Issue

Is SysManSMS Server and VISTA 5.1.7 tested on Windows 2008 R2 running in a Marathon EverRun Level 3 Solution?

Product Line

TAC Vista, Other

Environment

TAC Vista 5.1.7
SysManSMS Server

Cause

 The Server software is running on any Windows platform and release, including Embedded Windows..

Resolution

The SysManSMS Server is written is C and has no special requirements for the Windows platform. The Server software is running on any Windows platform and release, including Embedded Windows. The software has been certified by Microsoft for Windows 7, and tested for Windows 2008 R2.It will run in both 32-bits and 64-bits (compatibility mode) environments. The compatibility with TAC/Vista is no issue at all. The clean interface between Vista (writing Alert Files) and SysMan picking up the files to process will always work, We have more than 500 TAC/Schneider installations used with Vista. No reported problems.
Marathon EverRun Level 3 we do not know at all. As long as this software does not alter the above environments, it will for sure run.