Issue
Can the I/A Series R2 or G3 BACnet object_name be changed?
Environment
I/A Series R2, G3, UNC-410, UNC-520, ENC-410, ENC-520
Cause
The BACnet object_name property for an I/A Series R2 or G3 station is derived from a combination of the station name and assigned BACnet device instance number. For example, a station named BldgA with an assigned BACnet device instance number of 500 will provide an object_name of BldgA_500 upon BACnet request.
Resolution
The object_name cannot be modified by the user.