Issue
Aside from the recommended models from B&B Electronics, can Model # 485OT9L be configured to work with PSI 4.1?
Product Line
TAC IA Series
Environment
- PSI 4.1
- Network 8000 ASD devices (Microzone II, MicroFlo II)
Cause
On a jobsite and the only model available is the 485OT9L.
Resolution
It can work by using the following settings for the on-board configuration switches:
- Switches 1-4: 19200 baud (SW1=off, SW2=off, SW3=on, SW4=off)
- Switch 5: Echo off (SW5=off)
- Switch 6: Half-duplex (SW6=on)
- Switch 7: Half-duplex (SW7=on)
- Switch 8: Term Resistance (SW8=off)
- Jumper 1: JP1=SD
Note: Model # 485OT9L was discontinued by B&B Electronics in Sept. 2011