ENC-520 with 512MB of RAM

Issue

Can an ENC-520 be ordered with 512MB of RAM?

Product Line

TAC I/A Series

Environment

I/A Series G3 ENC-520 / ENC-520-2-N

Cause

The customer would like to have 512MB RAM in an ENC-520 instead of the standard 256MB RAM

Resolution

There is no option to order an ENC-520 with 512MB or any other RAM size other than 256MB. New ENC-520s ordered will be of the extended memory version and shipped with 256MB of RAM.
Also refer to related Lessons Learned article #7621