Issue
Unable to display Traditional Chinese characters when accessing graphics in an ENC via a web browser
Does I/A Series G3 provide non-English language support?
Environment
I/A Series G3 Enterprise Network Controller (ENC).
Cause
I/A Series G3 provides non-English language support by use of lexicons. Lexicons are identified by Java locale codes, such as “fr” (French) or “de” (German).
The lexicon 'Zh' was not installed into the ENC.
Resolution
I/A Series G3 provides non-English language support by use of lexicons. Lexicons are identified by Java locale codes, such as “fr” (French) or “de” (German).
The lexicon 'Zh' is for Chinese. This needs to be installed into the ENC.
- Open the ENC Platform.
- Expand Platform and go to the 'Lexicon Installer'.
- Click on the 'Install' button, select the lexicon folder you need and click 'OK'. The selected lexicon is now installed in the ENC.
* This article may apply to issues with other languages and not just Traditional Chinese.