Issue
Does the database file for a ProView display vary in size based on the amount of programming done to it with Niagara R2?
Environment
Niagara R2 all versions
ProView
Cause
Observation: A backup of an empty ProView display and a backup of a ProView display programmed with 30+ screens and dozens of bindings produced the same file size: 49 kB.
Resolution
No.
A backup database file from any ProView display, using the Niagara R2 wizard, will be 49 kB in size, whether the display is empty or has been extensively programmed.