How to use the Known Occupancy Count ( KnownOccupCount ) number of an Area in Plain English programming.

Issue

How to use the Known Occupancy Count ( KnownOccupCount ) number of an Area in Plain English ( PE ) programming.

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Continuum Access Control

Cause

Need to be able to retrieve the Known Occupancy Count number of an Area for use in Plain English programming for limiting access to an Area. The attribute does not show up in the list of attributes in  the Area Listview.

Resolution

Even though we can't see the attribute in an Area Listview, you can use the "KnownOccupCount" attribute at the command line or in Plain English programs.

 

Example 1 - Print Known Occupancy Count to command line.

print AreaFolder\Area1 KnownOccupCount

 

Example 2 - In a Workstations Program, set a pre-defined AnalogValue to the Known Occupancy Count of an Area.

Area1KnownCount = AreaFolder\Area1 KnownOccupCount

 

Note: The Known Occupancy Count will not function with Entry only doors. Both Entry and Exit readers are required on the doors within the Area. See Lessons Learned Article #7757 on this.