Issue
If the schedule for a personnel area assignment is in a different network to the door that uses the area it does not work.
Environment
ACX5740, ACX5720
Access Control
Cause
Objects can not be passed between different Continuum networks.
Resolution
For sites with 2 or more networks, when a schedule is linked to the area assignment of a person, that schedule must reside in the same network as the door that uses the area.
It is also good practice to locate schedules within the controller for that door, that way should it go offline the schedule will still operate correctly.