Issue
What is the Continuum 1.94 feature 'Editable SQL Admin Credential' as stated in the release notes?
Environment
Continuum Cyberstation v1.94
Cause
No explanation in the Release Notes or Product Announcement to explain what this new feature actually does.
Resolution
This new feature, is a change that allows a system to use an SQL admin account other than the SA account (built-in SQL system administrator account) to create a Continuum Database. In older version of Continuum this could only be accomplished with the SA account.
Now in Database Initialization, you have the option to select the SQL Admin user that you wish to use with the added Admin Username field. As per the image below.