Issue
Cannot upgrade CyberStation key.
Environment
CyberStation
Cause
Received key activation code from Repair Dept. to add an option to CyberStation. After entering the activation code into the KeyWriter application, getting the error "Invalid Key Activation Code: Please try again..."
Resolution
There is a KeyWriter application for the Continuum Reports Add-On Software and a different one for activation codes from the Repair Dept..
Use ...\Program Files\Continuum\CyberKeyWriter2.exe for the codes from the Repair Dept.