IP connections when TAC Vista communicate with a Xenta server.

Issue

Is TAC Vista creating a new IP connection every time it communicates with a Xenta server?  

Product Line

TAC Vista

Environment

TAC Vista 5.1.7 and earlier versions

Cause

When TAC Vista communicates with a Xenta server https is always used and a new connection is used every time Vista likes to communicate with the Xenta server.
When Vista is communicating with a Xenta 911 http is used and one connection which is connected as long as possible is used even if it is silence long period of times.

Resolution

When TAC Vista communicates with a Xenta server https is always used and a new connection is used every time Vista likes to communicate with the Xenta server.