In Niagara G3, the SNMP driver reference manual refers to three MIB files required so that the SNMP Point Manager can discover and add SNMP points as needed.

Issue

In Niagara G3, the SNMP driver reference manual refers to three MIB files required so that the SNMP Point Manager can "discover" and "add" SNMP points as needed.  The filenames are:

TridiumR3-MIB.my
RFC1155-SMI.mib
RFC1213-MIB.mib

Where can they be found?

Product Line

TAC I/A Series

Environment

Niagara G3

Cause

The three files are not easily located.

Resolution

The TridiumR3-MIB.my file is installed with the version of Niagara G3 installed on the host computer.

The other two files (RFC1155-SMI.mib & RFC1213-MIB.mib) can be found on the World Wide Web by searching using their specific filenames.

All three files are available here:  SNMP_Files_for_G3