Modulating actuator for VG221F

Issue

Which actuator is suitable for the MG221F valve when modulating control signal (0-10V) is required?

Product Line

Field Devices

Environment

VG221F

M800

M1500

Forta

Cause

There are a few different actuators listed in the VG221F documentation, but not all of them are available with modulating 0-10V control signal. 

Resolution

The Forta M800 and M1500 are both listed as suitable actuators for the VG221F, and both are capable of using the modulating 0-10V control signal.