Issue
How can I create a list view that will show only user activity where the user has deleted an object from the database?
Environment
CyberStation
ListView
Action Code
Cause
Need to research what items have been deleted from Continuum by others.
Resolution
- Create a listview.
-
On the General Tab configure the fields as follows.
- Class: Activity Event
- Filter: Today
- Path Type: AllPaths
-
On the Columns Tab add the following columns
- TimeStamp
- UserName
- NodeName
- EventObjectId
- Description
- Action Code
-
On the Qualifier Tab use the Query Wizard to configure the following attribute filter.
- Attribute: Action Code
- Operator: Is
- Value: 2