Issue
The ERR-block in Menta indicate that one or several switches on I/O modules are on manual control but they are not.
Environment
TAC Vista
Tac Xenta 400 with I/O modules
Cause
When this problem occur it is very unlikely that is a software issue, therefore the I/O module need to be replaced.
Resolution
Replace the I/O module.