Issue
Is it possible to download the Xenta 511 firmware to a Xenta 511-B?
Environment
TAC Xenta 511-B version 5.1.7
Cause
The 511-B version became obsolete in Vista version 5.1.5 as all Xenta servers got support for Modbus and the B stands for Modbus support. After version 5.1.5 it is only one firmware for the 511 and that is possible to download also to a 511-B.
Resolution
The 511-B version became obsolete in Vista version 5.1.5 as all Xenta servers got support for Modbus and the B stands for Modbus support. After version 5.1.5 it is only one firmware for the 511 and that is possible to download also to a 511-B.