Warning
Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support Services for assistance.
Issue
Large data base log file causes Continuum to run very slow and/or crash.
Environment
SU CyberStation
MS SQL Express
Cause
When Continuum starts and attempts to connect to the DB it takes too long due to the size of the log file (14GB in the case covered by this article)
Resolution
Shrink the database.
Go to http://technet.microsoft.com/en-us/library/ms190757.aspx for steps from Microsoft to shrink the database files.