Issue
User must not have access to change group access nor individual access.
Environment
All versions of I/Net software and OS.
Cause
If there are multiple Tenants in a building using the same software but the only changes that a user can make are those that they have access too and the others should be left alone.
Resolution
In order to resolve this, the following steps need to be followed:
1. Go to Edit/Host Computer/Passwords, select the user who the limitations would be set on.
2. Select Modify and on the bottom row there is a Tenant Button, it opens a Host Passwords - Tenants Editor.
3. Select a Tenant and verify that they have either Full or Limited Access.
4. If it is going to be limited, highlight and click on the Limited box, this brings up the Host Passwords - Groups Editor.
5. Select the box for Read Only access for which ever groups that access will be limited for and click on the OK buttons to close out.
6. Logoff then logon again as that user and verify that the limitations set about has been incorporated.