M1500 on a V232

Issue

Will a M1500 actuator fit onto a V232 valve?

Product Line

Field Devices

Environment

M1500

Forta

V232

Venta

Cause

Application assistance on Forta M1500 and Venta series V232 valve.

Resolution

The M1500 will fit, but since the V232 is only available in DN25,32, 40 and 50 size, we recommend using the smaller M400 or M800 instead.