Issue
Replacing a DC3000 controller.
Environment
Drayton
DC3000
Cause
The DC3000 is now obsolete.
Resolution
The DC3000 controller is obsolete, and there is no direct replacement available.
Our current range of discrete controllers cannot provide the same functionality as the DC3000, assuming that functionality has been used.
To provide the same controller functionality a programmable controller such as the Micronet or Xenta ranges will be required
To upload an overview of the Micronet range, please click HERE.
The Xenta controller range is listed as part of the TAC Vista Product Catalogue which can be downloaded from Schneider Electric but a table of the controllers and their I/O are shown below.