Issue
- Who edited an individual?
- Can I see in AMT who edited an individual?
Product Line
TAC I/NET
Environment
- I/NET
- AMT
Cause
When you want to know who last edited a individual you can track down this information in AMT.
Resolution
See the picture below. The first record, as an example, tells the following:
Device name: 001-00003 - 001 stands for "Tenant 1" 00003 stands for "Individual 3"
Event Type: Edit -Indiv. TAC - Tells that an individual was edited by user TAC
The editing user is recorded as the Initials assigned for the user; see image below.