Issue
In Niagara R2, when using the chart/log servlet in a browser, can the legend size be extended or widened?
Environment
Niagara R2
Cause
The name of log objects selected for a chart are truncated in the legend.
Resolution
The legend size cannot be adjusted manually. However, the descriptor used for the logged object can be customized somewhat.
When using the /chart/log servlet, use "Logs Only (Description)" or "Logs Only (Swid)", the Log Object's description displays in the Legend. There are about 26 digits available excluding units which can be used for customizing.
The descriptor field can also be cleared of any text and the /chart/log servlet will use the object's name in the Legend.