Issue
Enterprise Network Server station failed. Attempts to start the station resulted in the following error messages.
ERROR [15:32:36 04-Jul-12 SGT][sys] Cannot load station
java.io.EOFException
at javax.baja.xml.XParser.read(XParser.java:753)
at javax.baja.xml.XParser.parseText(XParser.java:621)
at javax.baja.xml.XParser.next(XParser.java:268)
at javax.baja.io.BogDecoder.decodeDocument(BogDecoder.java:164)
at javax.baja.io.BogDecoder.decodeDocument(BogDecoder.java:152)
at com.tridium.sys.station.Station.loadStation(Station.java:128)
at com.tridium.sys.station.Station.bootStation(Station.java:78)
at com.tridium.sys.station.Station.main(Station.java:978)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at com.tridium.sys.Nre.runClass(Nre.java:224)
at com.tridium.sys.Nre.main(Nre.java:149)
App Failed
Environment
I/A Series G3
Cause
The station's config.bog appears to be corrupted. The reason for this is unknown at this time.
Resolution
Restore the station database with the latest copy of a known good backup.