Cannot create ACWPPServerProxy application on the remote server.

Issue

Getting error cannot create ACWPPServerProxy application on the remote server when trying to use Web Pinpoint.

Product Line

Andover Continuum

Environment

WebClient

Cause

Configuration issue

Resolution

  1. Get the web.config file Download and place it in the Webservers. Do not edit this file with Notepad (Use Textpad ot Notepad++, etc.)
    • 64-bit systems directory: C:\Program Files (86)\Continuum\DNWACServerfactory (delete the old one)
    • 32-bit systems directory: C:\Program Files \Continuum\DNWACServerfactory (delete the old one)
  2. Reboot the Webserver.
  3. Start Continuum and edit any Graphic.
  4. Once the graphic is opened, select View / Options and set the Web locations. There shouldn't be any red X's
  5. Check the following file:
    • 64 bit systems:.C:\Program Files (86)\Continuum\DNWACServerfactory\ web.config  
    • 32 bit systems: C:\Program Files\Continuum\DNWACServerfactory\web.config
  6. The server  name should be correct.  It should match you Webservers name.

Now test Webclient on the webserver first before any client systems.

Make sure you run RegIIS and Caspol.exe 

C:\windows\Microsoft.NET\Framework\v2.0.50727\aspnet_regiis.exe -i

C:\Windows\Microsoft.NET\Framework\v2.0.50727\caspol.exe -m -addgroup Internet_Zone -zone InterNet FullTrust -name FullTrust

C:\Windows\Microsoft.NET\Framework\v2.0.50727\caspol.exe -m -addgroup Trusted_Zone -zone Trusted FullTrust -name FullTrust

Please note that the above may be case sensitive.