Continuum runs very slowly. Taking up to two minutes to first startup.

Issue

Continuum runs very slowly. Taking up to two minutes to first startup. Generally opening up Continuum Explorer and any other objects are seen to be slower than normal as well.

Product Line

Andover Continuum

Environment

Continuum v1.94 and above.

Cause

There was no Security Key connected and Continuum was running in Demo mode.

Resolution

Install valid Security Key and restart Continuum.

This symptom can also be caused by a missing or corrupt driver for the Security key, see Lessons Learned #4384 for details on re-installing the Security Key driver.

Note: Want to know what features are supported in Demo mode? Click here.