What is ADI Z-NET?

Issue

What is ADI Z-NET?

Product Line

TAC I/NET

Environment

  • ADI Z-NET
  • Graphic panels
  • Modbus
  • Smoke control systems

Cause

ADI Z-NET allows up to eight graphic panels to be interconnected as one larger Modbus interface port.

Resolution

ADI Z-NET is a proprietary network system / protocol that can interconnect up to eight graphic panels so that they appear as one larger (higher point count) MODBUS interface port. Refer to TCON 231: Smoke Control Systems Manual, ADI Z-NET for more information.