Is an existing IMI video frame grabber supported by Datacard?

Issue

Is an existing IMI video frame grabber supported by Datacard?

Product Line

TAC I/NET

Environment

Video Badging conversion from IMI to Datacard

Cause

IMI and Datacard are two different platforms with a defined upgrade path between them.

Resolution

The Flashpoint and Flashpoint lite, as most of the TWAIN devices are supported by the Datacard system. However, if the grabber card you have is not supported, a new card can be purchased from Datacard.