Setup Tap emulation on the HHC

Issue

What code do I use on the HHC to set the Tap emulation?

Product Line

TAC I/NET

Environment

Handheld Console

Cause

Setup Tap emulation.

Resolution

To set up Tap emulation:

  1. Press code 90
  2. Press [ENTER]
  3. Press the [INC] or [DEC] to toggle through 78010, 78035 or 78061 Tap emulation.

To set the baud rate for Tap emulation:

  1. Press code 91
  2. Press [ENTER]
  3. Press the [INC] or [DEC] to toggle through the available PC port baud rates. The baud rate is typically 9600 if connected to a host PC.

Refer to the appropriate controller TCON for more information.